This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR38020: Is there a controller(Using external FETS) with Vin 48V and similar functionality as LMR38020?

Part Number: LMR38020
Other Parts Discussed in Thread: LM5145, LM5148

Tool/software:

Hi,

I’m planning to use a PWM controller in My Buck converter application and use External FETS. Below are the desired specifications :

Vin : 48-52V
Vout : 12-36V
Pout : 1W- 24W
Fsw: 100k -1MHZ

I'm looking for a controller (Using external FETS) which has an external pin by which I can set the threshold to enter into SKIP/PFM mode at light load automatically. Does TI has a controller with these options?

I was looking at LMR38020 but it is not optimized for my application. 

Thanks!