Part Number: LMR36006-Q1
Other Parts Discussed in Thread: LMR36006, LM73606, LM62460-Q1
Tool/software:
Hi Expert,
There is an issue for LMR36006 design.
For our design requirement, we need FPWM for our system and which need SYNC pin pull up.
It was connected SYNC to Vin at REF SHC, after we filled in our design for our requirement.
But the maximum voltage limit of this pin is 5.5V while our Vin is 12V.
So, PMIC was break when we power on the system and find pin17 is short
Hope you can fix this bug to avoid other users meet same issue.
Below is schematic for your reference.