Tool/software:
Hello everyone,
I'm using the TPS25751D in my design to charge a 6-cell Li-ion battery pack via USB-C, with fast charging at 20V and 5A. I have a few questions about the setup and would appreciate any insights.
In my design:
- I've connected all VBUS and VBUS_IN inputs together and left the PP5V pins unconnected.
My question is about the VIN_3V3 (pin 36). Since the TPS25751D has a built-in 3.3V LDO, I’m not sure if the VIN_3V3 input needs a specific connection, or if it can be left floating. Additionally, with only USB-C as the power source, what would be the recommended source for 3.3V?
Any advice or recommendations would be greatly appreciated. Thank you!