This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5149: Dual Phases 30V and 15A: connections

Part Number: LM5149
Other Parts Discussed in Thread: LM5148

Tool/software:

Dear All,

we are designing a power supply with the following features:
--> Vin= 48V (-10%,, +15%)
--> Vout= 21..30V (28V nominal)
--> Iout=15A max

Because we uses the LM5149 for the other power supply, we want to use this chip.

PRIMARY CHIP:
--> Active EMI filter: Yes
--> Vccx: connected to external +5V
--> Rcnfg: 71k5
--> Rt: 82k5
--> PFM/SYNC: to VDDA
--> FB: Diveder of Vout
--> SYNCOUT: connected to PFM/SYNC of Secondary chip
--> EXTCOMP: RC filter connected to GND

SECONDARY CHIP:
--> Active EMI filter: No
--> Vccx: conneted to external +5V
--> Rcnfg: 90k9
--> Rt: 82k5
--> PFM/SYNC: connected to SYNCOUT of Primary chip
--> FB: connected to VDDA
--> SYNCOUT: float
--> EXTCOMP: connected to EXTCOMP of Primary chip
--> INJ and SEN: connected to REFAGND
--> REFAGND: connected to GND

The main question is if these connections are right or I forgot something...
Then, in the Seconday chip, do I need to connect Vccx to external power supply even if I don't use the Active EMI filter?


Thank You and Best Regards
Federico Battaglin