This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3895: Confirm if the capacitor value for the TPS3895

Part Number: TPS3895

Tool/software:

Hi AE,

        Please help check two question as below.

        1. According to the TPS3895 design specifications, when the CT pin is not connected to a capacitor, the default min delay time tpd(r)​ is 40 µs.

        2. When the target delay time tpd(r) needs to be set to approximately 105 ms, we can recalculate the required CT​ as follows:

       If CT is set to approximately 0.027 µF, a delay time close to 105 ms can be achieved.  Is it correct?
            
Best regards