Part Number: LP87524B-Q1
Other Parts Discussed in Thread: LP87524J-Q1
Tool/software:
I'm working with the LP87524J-Q1 PMIC and trying to enable BUCK0 by applying 5V directly to the EN1 pin, without using I2C communication. However, I am not observing any output voltage on BUCK0 under this setup.
When I enable BUCK0 through I2C, I can successfully read and monitor the voltage output. However, my goal is to activate BUCK0 simply by using the EN1 pin (set to 5V) as the manual suggests should be possible. Despite following the recommended wiring and configurations, BUCK0 does not output any voltage without the I2C setup.
I’ve attached the circuit diagram. Any advice on achieving direct control of BUCK0 through EN1 alone would be appreciated!

Please help me figuring this out