Tool/software:
Why R6 is not included in the Vout calculation?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
R6 value is only 49.9Ohm, which is small comparing to R7 and R8, has very slight impact to the Vout (3mV seen from below). We do not include R6 in the equation normally.
R6 | R7 | R8 | VOUT | calculation |
49.9 | 20000 | 10000 | 1.8 | 0.6*(1+R7/R8) |
49.9 | 20000 | 10000 | 1.802994 | 0.6*(1+(R7+R6)/R8) |
The 49.9 Ohm resistor is the injection resistor reserved incase the user need to measure the bode plot. Measuring Loop gain in power supplies.
Thanks and best regards.