Other Parts Discussed in Thread: LM5050-2
Tool/software:
Hi,
I am using the LM5050-1 to design a circuit that prevents current flow between two battery chargers when they are connected. I implemented an O-ring circuit with two LM5050-1 devices, but the ideal diode function does not seem to work as expected.
- When a battery (40–60V) is applied to the cathode, 8.7V is measured at the anode.
- When two chargers are connected, current flows between them. (In a circuit using the LM74700, both chargers detect the error and stop the current flow. This circuit worked well, but due to the low voltage rating, I wanted to use the LM5050-1.)
After repeating the above experiments, a spark occurred in the LM5050-1 on one channel. The device was damaged, and in another channel, the Gate and Source of the FET were shorted.
I will share the circuit diagram with you.
Thank you for your support.