Tool/software:
we are using BQ51003 IC for wireless charging on my device. In the Qi9WPC) specification, I'd like to the specification of temperature while the device is on charging via wireless mothode, Qi.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
we are using BQ51003 IC for wireless charging on my device. In the Qi9WPC) specification, I'd like to the specification of temperature while the device is on charging via wireless mothode, Qi.
now we are investigating on this temperature issue, it means the max temperature of Tx side goes up to 58 degree while it's on charging. I'd like to know the max temperature to make sure the device is safe in Tx and Rx side. It could be fine for Qi spec as well as Chip spec.
Hello
A thermal rise to 58 degrees is a little high, most devices want to keep the temp below 40C.
Have you built both the TX and RX?
Sure sir. both Tx and Rx used Ti Chip for Qi wireless charging system, and we can see the hightest temperature goes up to 58 degrees while it's charging. I'd like to know the specification of the Qi systems.
Hi
The Temp is high, and it is difficult to say what the cause is. It may cause problems for FOD test if you plan to certify the unit.