This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25149-Q1: Is there any way to enable active EMI filter in LM25149 even at light loads?

Part Number: LM25149-Q1
Other Parts Discussed in Thread: LM25149

Tool/software:

Datasheet says active EMI filter is disabled when load current is less than 30% of the current limit value. In my application i need a front-end converter to generate supply for push-pulls which then generate bias supplies for inverter switches. The load current here will be less than 30% of the current limit value for most of the time. So, is there any way to enable active EMI filter in LM25149 even at light loads?