Part Number: UCC14241-Q1
Tool/software:
Dear Specialists,
My customer is considering UCC14241-Q1 and has a question.
I would be grateful if you could advise.
---
I am thinking about using it for explosion-proof equipment.
IEC 60079-11:2011 is used for the standard required distance between the primary and secondary power supplies.
I am thinking of using Vin 24V → Vout 3V, Iout 0.4A.
The standard value of 30V will be used, so the following specifications are required.
Can the UCC14241-Q1 satisfy the following specifications?
(Between pins) Insulation clearance: 2.0mm
(Between pins) Creepage clearance: 2.0mm
(Inside IC) Insulation clearance: 0.2mm
I think the insulation clearance between pins and the creepage clearance between pins are satisfactory, is it correct?
I was unable to confirm the insulation clearance inside the IC in the data sheet, could you please let me know.
ーーー
I appreciate your great help in advance.
Best regards,
Shinichi