This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1A: Soc & SoH resolution

Part Number: BQ78350-R1A
Other Parts Discussed in Thread: BQ76920,

Tool/software:

HI, I have some questions.

I want to use bq78350-r1a with bq76920.

Trying to read data to SMBus by connecting MCU to bq78350-r1a.

1) Is it possible to read SoC data in 1% units through SMBus without representing it with LED?

2) Can SOH read the same way?

3) I want to read the data written below in real time. The application is a power tool(li-ion battery 5s2p 18v 8Ah).

  - cell voltage

  - charge/discharge current : 0~120A

  - cell temperature : -30 ~ 110 celsius

  - cycle counter

  - SoC : 0~100%(1% resolution)

  - SoH : 0~100%(1% resolution)

  Can I read all the data listed above in the bq78350-r1a & bq76920 configuration?

  Or do you have any other better ic configurations you can recommend?