Part Number: LP87725-Q1
Tool/software:
Hello,
I have tried the transient simulation for the LP87725-Q1 device but it doesn't run. Downloded the files from the product page directly and didn't modified anything. I get the following errors.
WARNING(ORPSIM-15246): Library index file LP87725-Q1_BUCK_TRANSIENT.ind does not have the correct format
INFO(ORPSIM-15422): Making new index file LP87725-Q1_BUCK_TRANSIENT.ind for library file LP87725-Q1_BUCK_TRANSIENT.lib.
Index has 10 entries from 1 file(s).
WARNING(ORPSIM-15256): <X_U1.X_U1_U3_U12.MNTYMXDLY> not a subcircuit param
WARNING(ORPSIM-15256): <X_U1.X_U1_U3_U12.IO_LEVEL> not a subcircuit param
WARNING(ORPSIM-15256): <X_U1.X_U1_U3_U12.TOL> not a subcircuit param
WARNING(ORPSIM-15256): <X_U1.X_U1_U7_U12.MNTYMXDLY> not a subcircuit param
WARNING(ORPSIM-15256): <X_U1.X_U1_U7_U12.IO_LEVEL> not a subcircuit param
WARNING(ORPSIM-15256): <X_U1.X_U1_U7_U12.TOL> not a subcircuit param
WARNING(ORPSIM-15256): <X_U1.X_U1_U12.MNTYMXDLY> not a subcircuit param
WARNING(ORPSIM-15256): <X_U1.X_U1_U12.IO_LEVEL> not a subcircuit param
WARNING(ORPSIM-15256): <X_U1.X_U1_U12.TOL> not a subcircuit param
ERROR(ORPSIM-15142): Node X_U1.U1_N00604 is floating
ERROR(ORPSIM-15142): Node X_U1.U1_U7_N13591 is floating
ERROR(ORPSIM-15142): Node X_U1.U1_N13510 is floating
ERROR(ORPSIM-15142): Node X_U1.X_U1_U3_U12.1 is floating
ERROR(ORPSIM-15142): Node X_U1.X_U1_U3_U12.2 is floating
ERROR(ORPSIM-15142): Node $G_DPWR is floating
ERROR(ORPSIM-15142): Node $G_DGND is floating
ERROR(ORPSIM-15142): Node X_U1.X_U1_U7_U12.1 is floating
ERROR(ORPSIM-15142): Node X_U1.X_U1_U7_U12.2 is floating
ERROR(ORPSIM-15142): Node X_U1.X_U1_U12.1 is floating
ERROR(ORPSIM-15142): Node X_U1.X_U1_U12.2 is floating
ERROR(ORPSIM-15143): Voltage source and/or inductor loop involving X_U1.X_U1_U7_U12.E_OUT1. You may break the loop by adding a series resistance