Other Parts Discussed in Thread: TPS65217
Tool/software:
Hi Team
below is my customer side requirement
Input Vbat=3V to 4.3 or 4.4V,always output is 1.8V or 1.9V.For the other three power rail,the VLED can be switch power source depend on charging or not,if on the charging this power rail will be from VBAT,but when charging is from VBUS.
The VPOD is 2V and other V30 for current source is 3.0V. and TYPE C input,but input power voltage is 5V level. Thanks!
do you have any recommendation ?
BRs
Brian