Part Number: TPS23882
Other Parts Discussed in Thread: CSD19538Q3A, CSD19538Q2
Tool/software:
Dear Sir
I have a sifos test for TPS23882 using SRAM_CODE_v15, but test fail
refer to following:

How should I solve it?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS23882
Other Parts Discussed in Thread: CSD19538Q3A, CSD19538Q2
Tool/software:
Dear Sir
I have a sifos test for TPS23882 using SRAM_CODE_v15, but test fail
refer to following:

How should I solve it?
Thank you
Hi Graeme,
Thanks for reaching out!
- Could you share your schematic?
- You may try to enable / disable the alternative inrush

- The MOSFET selection could be a cause of such failure. Could you share MOSFET datasheet? It is better to be or close to CSD19538Q3A with below features
|
Characteristics |
Impact Factor (not qualified) |
CSD19538Q2 |
|
Gate Resistance |
* |
4.6 Ω (typ), 9.2 Ω (max) |
|
Vgs Threshold |
***** |
2.8 V (min), 3.2 V (typ), 3.8 V (max) |
|
Transconductance |
*** |
19 S |
|
Ciss |
** |
349 pF (typ), 454 pF (max) |
|
Crss |
** |
12.6 pF (typ), 16.4 pF (max) |
|
Qg |
** |
4.3 nC (typ), 5.6 nC (max) |
|
I-V Characteristics |
***** |
Figure 3-2, 3-3, 3-7 |
Best regards,
Diang
Hi Diang
The alternative inrush is disable by defalut setting.
The MOSFET datasheet and schematic refer to PDF
TPS23882.pdfCRMKTL10120A_Datasheet_V1.0.pdf
Best regards
Hi Graeme,
This FET has a very low Vth. Could you try one with >= 2V min Vth?

Best regards,
Diang