This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8865Z-Q1: microcontroller with CAN bus

Part Number: LP8865Z-Q1
Other Parts Discussed in Thread: MSPM0G3507-Q1

Tool/software:

I am looking for an AEC-Q100 grade 1 qualified microcontroller with one CAN controller, NOR Flash, ISO 26262 ASIL B, and able to interface with at least 2 LP8865Z Drivers. Other desired features include watchdog timer, slow clock detect, brown out reset, ECC single error detect & correction and double error detect, DAC output. Looking for something that is somewhat radiation tolerant: SEE LET minimum threshold > 37 MeVcm2/mg.

A SPI interface and/or a I2C interface is desirable. Some discrete peripheral I/O is also desired to read the Fault of the LP8865Z.

Can you recommend something?