Part Number: LP8732-Q1
Tool/software:
Hi team,
LP8732-Q1 has the soft start function on LDOs, but users cannot configure the soft start function. Is my understanding correct?
Best regards,
Shunsuke Yamamoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP8732-Q1
Tool/software:
Hi team,
LP8732-Q1 has the soft start function on LDOs, but users cannot configure the soft start function. Is my understanding correct?
Best regards,
Shunsuke Yamamoto
Hi Yamamoto-san,
The soft start feature of LP8732-Q1 is used to describe the behavior of the BUCKS, starting up from 0 V → 0.35 V before the slew rate control.
This is not configurable. This is a built-in function.
The LDOs do not have a soft start feature, as this is not typical for LDOs. The typical startup time for LDOs is 300 us, including delay and slew rate is ~15 mV/us, this also cannot be changed.

Best Regards,
Sarah