This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1825: Availability of screening test

Part Number: UC1825


Tool/software:

Hi team,

The customer is experiencing problems with the UC1825L883B.

The UC1825L883B operates normally at normal temperatures, but at high temperature (ambient temperature + 60°C), the OUT A and OUT B pins' PWM output width decreases, causing a drop in circuit output voltage.

Voltage and current feedback that decreases the PWM output width of the OUT pins when an abnormality occurs is not confirmed.

Please refer to page 18 “4.2 Screening” of the document at the following URL.

https://landandmaritimeapps.dla.mil/Downloads/MilSpec/Smd/87681.pdf

It seems that screening test according to MIL-STD-883 method 5004 is conducted, are all devices screening tests conducted during pre-shipment testing?

Thanks

Best regards,

Masahiro Kobayashi