This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25758: BQ25758 OCP Notification via INT pin

Part Number: BQ25758


Tool/software:

Hi,

Recently I have started using BQ25758 which is available in Thunderbolt design, and configured IOUT_REG to trigger OCP at 1A current by programming IOUT_REG with value 0x0050.

When OCP occurs, I see that the INT is triggered.

However when we read 0x21 to 0x24 it shows the below values

0x21 = 0x03, 0x22 = 0x80, 0x23 = 0, 0x24 = 0.

I thought that IBAT_OCP should have set when OCP occurs.

Could you let us know how to detect when there is OCP when BQ25758 is operating in Buck / Boost modes ?

Regards,

Sudheer