This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GPCCHEM: No ChemID with DOD deviation below 3%

Part Number: GPCCHEM

Tool/software:

I have performed a cycle on cell according to slva725a guide for selecting a Chem ID and uploaded to GPC Chem Tool.

The report I got back found a chem ID of 3567 with 5.6% deviation as the best match.

What does that 5.6% mean - is the maximum error between the voltage of 3567 and the tested cell at the same SoC?

Is there a way to tell where the worst mismatch occurs - i.e. at the start of discharge (less important in our application) or at the end of the discharge (more important for our application)?