This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62914: Efficiency curve different in WEBENCH Power Designer

Part Number: TPS62914
Other Parts Discussed in Thread: LM62460

Tool/software:

Hi,

My use case is 12V input and 5V (up to 4A) output. The Efficiency vs Load curve (12V input, 5V output, 2.2MHz switching) given in the datasheet and the WEBENCH Power Designer is off by about 5%. Datasheet shows about 90% efficiency and WEBENCH shows about 96% efficiency at 4A output. Am I missing something?

Thanks!