This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25890: Power limited of the BQ25890 cuases failure

Part Number: BQ25890


Tool/software:

Hello

I am design a system that using the BQ25890 for the battery management. But I my CPU power up cuased by a power limited of the BQ25890.

The boards work fine for a PD power which can output 12V.

But it fail when I use the RPI5 adapter which can output 5V/3A.

After some debuging, I think it is cuased by the BQ25890 to limited the adapter to 500mA then cuased the VSYS lower than 3V. But my system need more than 500mA for boot up.

I design the divider 4 follow the datasheet which can set the power limited to 2.4A, I can measure the 2.68V on both D+ and D- pin of the BQ2590, but it seems that does work, the board still power up fail !

Can anyone help on this? Urgency

My design bellow: