This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B86-Q1: Expected Vout rise rate

Part Number: TPS7B86-Q1

Tool/software:

What is the rise time of Vout when EN = Hi?

Please let me know the time for three pattern of Vout percentage below.

[1] 10% -> 90%

[2] 10% -> 60%

[3] 10% -> 40%

circuit conditions:

  Vin = typ.13.5V(range: 9~16V)

  Vout = 5V *We use fixed model.

  Iout = 0mA

  Cout = 10uF

  TJ = –40 to +150 degree