Tool/software:
What is the maximum power consumption of the TL594?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Its Tj,max = 150C, so to determine the max power the IC can do, you need to calculate all power on the pins then find if the resulted junction temperature is within 150C.
With only consider the static operation, based on the datasheet: Vcc x the listed current is the IC allowed max power in static condition.