Tool/software:
Hi,
I have a problem with the TPSM365R6. The 5V output voltage oscillates like on the oscillogram below.
The input voltage range is 12-48V. The oscillograms were done with 25V on the input.
Here is the scheme:
The load is the MCU and some digital peripherals, with the LDO to make 3V3.
Layout:
top
2nd layer - gnd
3rd layer:
bottom:
I suspect that the connection of the 5V to the FB line by the via to the 5V polygon may cause problems. Do you think that a shorter connection directly to 5V output pad could solve the problem?
The converter is unstable. It helped when we initially changed the capacitors from 10u to 22u, which reduced the oscillations, but the problem wasn't solved. Three additional 22u capacitors didn't change the behavior—we observed a small, insignificant improvement. What can be the reason? The power supply is a good-quality bench supply; we also tried with the battery.
What can be the reason for the oscillations and how to solve the problem?
Best regards
Lukasz