Tool/software:
Hi TI Experts
We use LM51227 in wireless power charger in auto.
The datasheet described the Vo can dynamical progarming via I2C from:
-3.3V up to48V in20 mV steps
-1V up to 24V in 10mV steps.
The question is:
If we chose 10mV steps to set Vo at 24V in chargering phase, then,if we need more higher Vo, can we set steps to 20mV in order to set Vo at 26V?
It`s free to switch this two steps in a charging phase, and this operation will not to turn off the charging function?
The charging process is continuous during the voltage step transition, right?