Part Number: LM117HVQML-SP
Tool/software:
Hi,
I am using the LM117HVQML-SP in a system that can see input voltage transients of up to 75V. Can the LM117HVQML-SP take transients of this high, say if the transient is 75V, 20V/us, and 10us total pulse width? Can the regulator handle these types of transients, or would any input voltage above the rated 60V cause permanent damage?
Thanks!