Other Parts Discussed in Thread: BQSTUDIO, , EV2400
Tool/software:
Hi TI,
Searching the E2E forums, it appears the address is 0xAA (or 0x55 without the read/write bit). I've a BQ78Z100 that I'm able to communicate with via BQSTUDIO and an EV2400, but cannot see the device when performing a 7-bit I2C scan. Can see other devices on the I2C bus, but nothing shows for the BQ78Z100. My device is sealed from the manufacturer, not sure if that has anything to do with it. Is there anything specific to a sealed BQ78Z100 that needs to be done to see it via I2C?