Other Parts Discussed in Thread: TVS2700, TVS2200, TPS25948, TPS2663
Tool/software:
Hi,
I'm working on a compact board that uses both 14V and 24V rails. It has three voltage rails, one for 24V and two for 14V and needs protection against over-current, over-voltage, under-voltage, and possibly reverse current.
I'm considering using three TPS25983 devices as fuses (one for each connector) with reverse-blocking MOSFETs. I'm also planning to add TVS diodes on the outputs for transient and ESD protection. The 14v rails have a max current of 6 amps and the 24v rail has a max current of 4 amps.
Here's my issue:
-
24V Rail Protection: The TPS25983 has a max voltage rating of 30V, which doesn't leave much room for TVS diode selection. I considered the TVS2700 flat clamp, but its max clamping voltage is 32V—above the TPS25983's limit. However I think The 14V rails are fine with the TVS2200.
-
Space Constraints: The board is very tight on space, so adding ideal diode controllers and MOSFETs instead of the TPS25983 might not be feasible because of size.
-
It seams to me the issue mainly arises when the reverse-blocking MOSFET is on. If it's off, the TVS2700 would be acceptable due to the MOSFET's higher voltage rating.
My Questions:
-
Any suggestions for protecting the TPS25983 from transients at 24V, considering its 30V max rating of TPS25983?
-
Is there a way to tweak the circuit to get proper transient protection without exceeding voltage limits? Maybe adding a comparator to the reverse blocking diode to detect transients and quickly shutdown the reverse blocking mosfet?
-
Are there compact alternatives to the TPS25983 that could fit within my space constraints?
I chose the TPS25983 mainly for its small size and integration with the reverse-blocking MOSFET. But given the space limitations, I'm open to other ideas.
Thanks in advance for any advice!