This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79600-Q1: bq79600 reverse ring communication

Part Number: BQ79600-Q1


Tool/software:

Hello, I am establishing communication with bq 79600+ 8 bQ79612 in the north direction via uart, the hardware required for ring communication is also installed as hardware. 



this code is my bq init code, so I can read voltage data from the modules I want, but in case of cable breakdown, I should also use the reverse part, for this I have a code with the following commands, but I cannot provide reverse reading, I added all the commands by reading them from the datasheet, but is there something missing?