Part Number: BQ40Z50-DEVICE-FW
Tool/software:
Hello forum.
I have a rather special question for a specific use case in which it is desired to limit the battery voltage from the normal operating voltage limit.
Say that I for protection reasons wants to limit the battery operating voltage from the normal operating range (3.0V - 4.2V) to something like 3.0V - 3.8V. In this reduced voltage operation range:
- I want to display the new max voltage, 3.8V, as 100% SoC instead of 4.2V
- I do not want the Impedance Tracking / learning algorithm to use any data in this stage for improving its learning registers.
My question is therefore: Can the above be accomplished, where the learning algorithm of the BMS ignores the reduced operating range until this mode is exited? Will the learning algorithm / IT data be preserved when going back to normal mode?
Ignore the transition between these two stages for now, e.g. if the battery voltage is above the new operational limit, this will most likely be fixed through a burn script when entering this mode.
Hope the above makes sense, and please reach out to me if anything needs to be elaborated.
Thanks in advance
Kind regards,
Victor