This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118: LM5118 : buck boost converter output regulation issue.

Part Number: LM5118
Other Parts Discussed in Thread: LM5170

Tool/software:

LM5118 Buck boost converter

We follow all the steps for the design for LM5118 buck boost converter, however the output regulation is not maintained. specifications: Input voltage range 8V to 30V DC. and output is 10V ,1A.

I am getting 4.37V output when the input 12V is given. Also, it does not maintain the regulation.  When I give 24V DC input, output is 6.25V output. Pls suggest.