This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62585: The max output capacitor

Part Number: TLV62585


Tool/software:

Hi team,

This is FAE Jayden, My customer is using TLV62585 and they have the same question with the previous E2E thread.

The work condition is: VIN=5V, Vout=3.5V, Iout=0.95A, L=1uH, Cout=200uF

Can this device support 200uF output capacitor considering the inrush current and loop stability? Thanks.

Brs

Jayden