Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

TPS1641: Vcc reset - what are the timing requirements?

Part Number: TPS1641

Tool/software:

My customer is using the TPS16412 and wanted to recover from a latch off condition using Vcc instead of EN/SHDN pin. The datasheet does not seem to cover this aspect - what are the requirements for switching off Vcc? Is it the same timing as EN/SHDN? What is the low voltage threshold?

In the customer's design, the fault occurs when the input voltage droops from 17V to about 7V and then back up to 17V. Right as the voltage begins to rise back up to 17V the fault line trips and stays tripped. This happens in roughly a 10ms transient. They are working to implement a patch to reset the device by cycling Vcc.

Thank you!