Tool/software:
Hello, I was wondering if I use the LM5148 as it is to drive GAN transistor with max Vgs of 5.5V. In case if it is possible what should I be carefull of? I was thinking about creating a 2.2MHz buck converter from 48V to 20V.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello, I was wondering if I use the LM5148 as it is to drive GAN transistor with max Vgs of 5.5V. In case if it is possible what should I be carefull of? I was thinking about creating a 2.2MHz buck converter from 48V to 20V.
Hello Godziller
Since LM5148 regulates VCC voltage which is the source of low-side MOSFET driver, at 5V+/-0.3V, the maximum V(LO-GND) voltage can be well regulated. But V(CBOOT-SW) which is the source of the high-side MOSFET, can be greater than V(VCC-GND) when the SW node negative spike is greater than one diode voltage drop. Please optimize the PCB layout in order to minimize the negative spike.
-EL