Tool/software:
Dear,
Could you please help me check the shutdown activation circuit of the High-Side Protection Switching Using N-Channel MOSFETs?
1. May I ask if the voltage of the battery cell can be charged and activated if it is below 1.8V?
2. After shutdown, it will reset again when charging is activated.
What will happen to the MOS(Q2/Q3/Q4/Q5) transistor in this situation? Will it immediately activate charging? Or will the MOS transistor not activate?