This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25172: Fast Charging

Part Number: BQ25172

Tool/software:

Dear Team,

My customer is evaluating the BQ25172EVM to charge 1-cell NiMH batery (1.2V, I_charge: 500mA) under VIN=5.0V (USB VBUS). When it is initial charge, the charging current need to be change at V_bat=1.1V. So, the charging current setting need to be changed by monitoring the battery voltage.

Can the BQ25172 be used for fast charging with I_charge=500mA?

Best Regards,

Koshi Ninomiya