This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62932: Need an Alternate part with Isolated output.

Part Number: TPS62932


Tool/software:

Hi Team,

We are using TPS62932DRLR, DC-DC Buck converter in our designs.We are looking for an isolated switcher or module, As this module is not supporting isolated Vout.

Please suggest an isolated part with the below specs.

Vin min - 23Vdc
Vin Max - 23Vdc

Vin Nom - 24Vdc

Vout - 12Vdc
Iout Max 2A

Iout Nom - 0.6A

Note : Output has to be isolated one. Max ripple allowed 1%.