Tool/software:
Dear TI ,
I want to use the Texas Instrument "Wireless Power Receiver" in the main device which is Bluetooth based FDA certified Medical class 1 device and "Wireless Power Transmitter" for the wireless charger which can be charge the device. In the existing design (which was designed approx. 15 year of ago in US) , now we are in the re-designing phase for that same device. In the existing design the receiver and Transmitter used with Renesas Make. Part No. P9027LP-RAWGI8 Description: IC WIRELESS PWR RECEIVER 40WLCSP
Part No. P9235A-RNDGI8 Description: IC WIRELESS TRANSMITTER 48QFN. Now the both part has been obsolete of Renesas make and they have no alternates against the same.
Now, we want to use the Texas Instrument Wireless power receiver & transmitter as well. We need your prompt support for the same to move ahead in this re-designing phase. Hope you will support on ASAP.
Looking forward to your response.
Thanks & regards,
Tajwar Chandel
Mob. No. +91 985 73254 11
Email id;- tajwarc@zimetrics.com