Part Number: TPS61071-Q1
Tool/software:
Hello,
I am an FAE at a distributor that handles TI products.
I asked about the issue of the SW pin being shorted to ground in the following thread.
I received a follow-up question from my customer.
The symptoms of the circuit are as follows.
A voltage (about 7.7V, 20us to 50us pulse) exceeding the absolute maximum rating (7V) was applied to the SW pin.
(Question 1)
Shouldn't the absolute maximum rating be exceeded, even for a momentary pulse (overshoot) of 20us to 50us?
If the rating is exceeded, will it only affect the product's lifespan, or will it immediately lead to electrical destruction?
(Question 2)
If there is a margin for the absolute maximum rating, I would like to know how much it is.
(Question 3)
What kind of failures are possible if the absolute maximum rating is exceeded?
Best regards,