This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2813-5: Support and confirmation on UCC2813 suitability in -40deg.C application

Part Number: UCC2813-5

Tool/software:

Hello,

For DC to DC battery charger application, considering using UCC2813-5 in 2 location, one as aux power supply and second for battery charging in 2 switch forward topology.

Application is battery charging in CC CV mode.

Ambient temperature range is -40deg.C to +50deg.C

Input voltage :- 20V to 30Vdc

Output voltage: - 14Vdc

Appreciate your guidance / confirmation whether UCC2813-5 can be used.