This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM53602: Pspice simulation issue.

Part Number: TPSM53602


Tool/software:

Hello,

I'm trying to simulate the TPSM53602 power module with the following parameters:

  • Vin = 5 V
  • Vout = 3.5 V
  • Iout = 1.5 A

There is no output voltage present, even with a valid input voltage and an EN voltage above the threshold. All simulation settings are default. I’m attaching files and screenshots.

TPSM53602.zip