Tool/software:
Hello, E2E forum!
I would like to ask you one question regarding the EVM board.
I am planning to test the 1SnP battery configuration using BQ76952EVM board.
Since I previously communicated with CSC regarding this matter, I already know that using '1SnP only' is not possible.
In that case, I would like to ask you about the method below to see if method below is possible to perform the experiment.
If it's not possible, can you tell me why it is not possible?
a) Connect DC power supply to the BQ76952EVM using "Cell16" and "BAT –" terminals for power support.
- I am guessing BMS needs some amount of power support to operate properly.
b) Short BQ76952EVM's "Cell 2 ~ 15" terminals because I am not trying to use these.
c) Connect 1SnP Configuration to the BQ76952EVM's "Cell 1" and "BAT – " terminals for the experiment.
d) Make sure DC power supply and 1SnP setup's ground voltages are same to prevent possible issues.
Regards,
TJ Chae