This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22992: VIN and VOUT pin is too close, is the dimension diagram correct?

Part Number: TPS22992

Tool/software:

dears,

my customer is working on the PCB design with TPS22992,  they are concerning the distance between the VIN and VOUT pin is too close, so might lead to the risk of short-circuit:

according to the package dimension diagram, the chip width is 1.25mm, the single pin width is 0.4-0.6mm, and the gap between the middle value is only 0.25mm, considering the maximum tolerance, it will be short-circuited.

would you please help to double check if the dimension diagram of RXP0008A package is correct?

thanks!