Part Number: LM5060-Q1
Other Parts Discussed in Thread: LM76202-Q1, LM5060
Tool/software:
Hi,
I have a worked a schematics using LM5060-Q1 for the below mentioned specification, does this looks fine or any improvement needed in the design.
| Design specifications | |
| Input voltage | 9-16V |
| OVP typical | 18V |
| UVP typical | 9V |
| Current max | 1A |
The output of LM5060-Q1 goes to a Buck regulator. End application is a rear view camera used in an automobile
Also we are testing the boards as per,
ISO 7637-2 Pulse 1(-150V) and Pulse 2a(+112V)
ISO 16750-2 Load dump Test B with centralized load dump suppression.
Also ,I need some clarification regarding the working of the sense pin and the calculation of Rsense for understanding purpose, the use of Rsense is to limit the output current or any other.