Tool/software:
Hi,
I am using the LDO output of the BQ34Z100-G1 as the supply for a PIC microcontroller. During programming of the PIC, I need to be able to supply the PIC from the programming tool (so that the programming voltage and Vdd can be applied in the correct sequence). If the BQ34Z100-G1 is powered down, will applying 2.5VDC to the REG25 line cause any damage? Unfortunately, I don't have the option of adding a jumper to isolate the supplies.
Many thanks,
Adrian