Tool/software:
Hi TI Forum,
I have designed the following circuit (below), but I'm not totally confident regarding the TVS selection and/or my understanding of the datasheet. I was hoping this could be validated and if incorrect, suggest how I can correctly implement it(?). Please note, BATT is just a standard Li-Ion 40V battery.
1) Is my setup of two uni-directional diodes ok? Is it possible to just use one bi-directional diode without losing RPP functionality?
2) It was very difficult to find a diode that meets both the working/clamping voltages. Hence, I 'assume' given that it's only for transient conditions, a clamping voltage of 69.8V (just 0.2V under the device maximum) is 'ok'?
3) What is the likely output current of SW? The op-amp has I(max) of 5mA (Vin+/Vin-), hence I added a 1kOhm resistor, but is this needed?
4) Is there anything else that I've forgotten?
Many thanks,
Darren