Other Parts Discussed in Thread: PMP40933, PMP40934, TPS25772-Q1
Tool/software:
Hi
After some issues I got my design working. USB PD is reporting correctly to the sink and port orientations is detected.
Now I got a new issue. When requesting more than 13.5V the output just shuts of, even with no load.
I've tried a USB tester, JOY-IT JT-UM120, to request outputs from the IC and it works beautifully until I try to get 13.6V or more.
i've also tried with a Valve Steam Deck that wants up to 3A @ 15V, but it does not start charging, the input current to the board just jumps around a bit.
Here I can also use my USB tester to see the voltage and current readings. Voltage matches my oscilloscope
I've a voltage offset of about -8 here to get a better view of it waveform.
As we can see, it goes up to 5V, sen it tries to go for 15V but fails.
What else can I test?