Other Parts Discussed in Thread: DLP4500, TPS7A37, TPS56C231
Tool/software:
Hello
We design a replacement LED driver for the DLP4500 for delivering 10A LED current using the TPS56A37
The LEDs are connected in current loop and basic driver is working driving the LED with 10A current
We encountered issue with ON / OFF loading the driver (MOSFET switch) ,
When we draw a small amount of current (low intensity) the TPS56A37 switch to work in light load (ECO-MODE) condition cussing the LED to flicker
and when we increase intensity the TPS56A37 lock into light load (ECO-MODE) state and keep flickering,
We have some thought of loading the output of the TPS56A37 continuously, but we are not sure whether its the right way, since we work in current loop and the equation on page 12 in the datasheet (for finding the load current to switch off ECO-MODE) use output voltage not current .
Is there is a batter way to disable the light load state and keep the TPS56A37 in full work state even when the load (LED) is disconnected or to find a load current to place the TPS7A37 in full work load?
P.S. current loop is done connecting the LED from the TPS56A37 output through a 25m ohm sense resistor and feeding the TPS56A37 FB pin with the voltage sampled by the sense resistor.