This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478: Use boost converter for charging battery with BMS

Part Number: LM3478

Tool/software:

Hello

I am designing a solar harvesting power supply with a Talentcell 6V 6Ah LiFePO4 Battery Pack. The battery has protection for over-charge, over discharge, over current and over temperature. If the battery is treated as open circuit for over-charge protection, would the LM3478 boost converter go into shutdown mode or continue running? If the LM3478 is still running, is it safe to operate under open/short circuit conditions? Can this charge controller be used for non-static loads?

The design will have a Vin of 4-5V and output 7V/2A.

Thank you for your help.

Travis